AXIS#.SAFE.SCA_#.INTERNALSTATE

Description

Indicates the internal state of the Safe CAm (SCA) function state machine.

Value Description

0

Not in range

1

In range

Context

For complete SCA information refer to AXIS#.SAFE.SCA_#.INTERNALSTATE.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read Only

Units

N/A

Range

0, 1

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No